Сегментация сети
Increase network security and improve user experience by segmenting the network
Modern networks must support an ever-increasing number and diversity of devices. Often these are unmanaged devices, including BYOD and guest devices, that can be risker than those owned by IT. IoT devices may also be especially vulnerable to security threats. Absent any means to prevent them, security threats can readily propagate horizontally within the network environment once they have penetrated the network perimeter.
Device proliferation can also contribute to a poor user experience, particularly in certain industries such as multi-dwelling units. Users have visibility into devices that are not relevant to them, and this can create confusion. Data-intensive applications accessed by visitors may compete for bandwidth with mission-critical applications. Network segmentation—or the practice of dividing the network into multiple smaller subnetworks—can help address these challenges.

Stronger IT security with multiple virtual networks to separate devices
IT teams can improve the security posture of the network using network segmentation to isolate certain devices and groups of devices from others. This can keep threats from propagating on the network. Unmanaged and IoT devices can be placed upon their own virtual networks to mitigate the risk. That means that, if a device connects that is affected by a security threat, it won’t be able to infect other devices that are on a separate virtual network. IT can grant guest users internet access only on a separate guest network. Network segmentation can also isolate users and devices that are subject to stringent compliance requirements, making it easier to meet these requirements.

Virtualized personal networks for a better user experience
Network segmentation can help IT teams deliver a better, more personalized experience for users. This is especially true in multi-dwelling units, including in higher education. CommScope RUCKUS® enables IT teams to segment a single physical network into multiple virtual networks—even down to the level of individual users. Since each user is on their own virtual network, they only see the devices that are relevant to them. They can roam about the network environment and still be connected to their personal virtual network. IT teams can also use network access policies to prioritize mission-critical data traffic—providing superior quality of service where it matters most to the organization.

Deployment options to support any network—whether or not it’s a RUCKUS network
CommScope offers two technologies within the RUCKUS product line to enable network segmentation—VLANs and VXLANs. VLANs can be employed whether or not the underlying network is a RUCKUS network, and this approach scales to about 4 000 separate virtual networks. RUCKUS Cloudpath® Enrollment System enables this capability. VXLANs have much higher scalability than VLANs, and enable virtual networks than span physical network segments. Deploying VXLANs on a RUCKUS network requires a SmartZone™ controller, SmartZone Data Plane and Cloudpath Enrollment System. RUCKUS products automate many tasks associated with setting up VXLANS to dramatically simplify the process.
Основные ресурсы

Видео. Сегментация сети
Сегментация сети — это практика разделения корпоративной сети на более мелкие подсети. Она изолирует пользователей и устройства друг от друга для повышения ИТ-безопасности и удобства работы пользователей. Сети Ruckus помогают упростить сетевую сегментацию в любой сети и обеспечивают еще более широкие возможности сети RUCKUS.
Пример использования у заказчика: AVE Union
AVE Union — это комплекс апартаментов премиум-класса в Юнионе, штат Нью-Джерси. Компания выбрала сеть RUCKUS для обеспечения быстрой и бесперебойной работы Wi-Fi. Система регистрации в Cloudpath позволяет жителям быстро и безопасно подключаться к сети. Новая сеть — это конкурентное отличие объекта недвижимости.

Мини-вебинар по требованию Сегментация сети
Этот мини-вебинар по требованию охватывает сегментацию сети, технологии, поддерживающие ее (VLAN, VXLAN) и сопутствующие RUCKUS продукты. В ходе него также рассматривается специализированный вариант использования виртуализированных персональных сетей в секторе многоквартирных домов (MDU).
Краткий обзор решения. Сегментация сети
This solution brief describes supporting technologies and use cases for network segmentation.

Дополнительные ресурсы

Видео. Сегментация сети
Сегментация сети — это практика разделения корпоративной сети на более мелкие подсети. Она изолирует пользователей и устройства друг от друга для повышения ИТ-безопасности и удобства работы пользователей. Сети Ruckus помогают упростить сетевую сегментацию в любой сети и обеспечивают еще более широкие возможности сети RUCKUS.

Network Segmentation Mini-Webinar
Этот мини-вебинар по требованию охватывает сегментацию сети, технологии, поддерживающие ее (VLAN, VXLAN) и сопутствующие RUCKUS продукты. В ходе него также рассматривается специализированный вариант использования виртуализированных персональных сетей в секторе многоквартирных домов (MDU).

Видео. Сегментация сети
Сегментация сети — это практика разделения корпоративной сети на более мелкие подсети. Она изолирует пользователей и устройства друг от друга для повышения ИТ-безопасности и удобства работы пользователей. Сети Ruckus помогают упростить сетевую сегментацию в любой сети и обеспечивают еще более широкие возможности сети RUCKUS.

Network Segmentation Mini-Webinar
Этот мини-вебинар по требованию охватывает сегментацию сети, технологии, поддерживающие ее (VLAN, VXLAN) и сопутствующие RUCKUS продукты. В ходе него также рассматривается специализированный вариант использования виртуализированных персональных сетей в секторе многоквартирных домов (MDU).