Data center networks a la "mode"

James Young James Young October 31, 2017

Data Center 360x203Data center networks are under pressure to evolve to provide higher capacity. This applies to virtually all types of networks. Over the last few years, many use more fiber optic cables and transceivers to the point that fiber optics is now the default choice. Clearly the trend is to higher-speed fiber optics.

The design of data centers with higher capacity and optimal cost is evolving. One of the hot topics is what type of fiber to deploy: multimode or singlemode. The fashionable answer is to deploy singlemode cabling, the kind that long-haul telecom and transoceanic networks use.

Yet in data centers, singlemode cabling is only recently making a significant entry. While singlemode systems are great for long distance networks, they have traditionally been expensive and power-thirsty when compared to multimode, the workhorse of data center networks. Some network operators advocate that singlemode is destined to replace multimode due to its superior bandwidth. But many operators prefer an analytic versus trendy approach.

CLICK TO TWEET: Differences between multimode and singlemode fiber? CommScope's Jim Young breaks it down a la "mode."

There is a significant demand for longer distance support in larger hyperscale data centers, which is not generally the case for enterprise data centers. Singlemode is better at longer distances, and if the cost can be trimmed, then perhaps it is a good choice for larger data centers with a need for much higher capacities. On the other hand, if multimode can also deliver higher capacity with acceptable distance support and competitive costs, then there are reasons to continue with it.

A typical considerations list for data center networks looks a bit like this:

  • Support for the distances and connections
    • Some need 500m and some need less than 100m
    • Some need point-to-point cabling with few connections, while others want the reconfiguration benefits that a structured cabling approach delivers.
  • Capacity
    • Some need 400G or more and others are happy with 10G
    • All agree that more capacity will be required in the future
  • Supply risk
    • Some are okay with limited supply scenarios
    • Others need the supply assurance of standards-based solutions
  • Upgradability
    • Some have multi-generational evolution objectives
    • Others have a more limited upgrade expectancy before replacement
  • Cost
    • Everyone wants low cost
    • The issue here is how to measure the true cost of the various options over time

DC chart 360x203Some data helps evaluate these listed items. Here, looking ahead a bit at the relative cost of 100G data center network options, the cost of the channels, including transceivers and cabling, is shown as a function of channel length. This provides guidance for the technologies you might consider deploying in your data center.

Comparing this graph to that of slower data rate solutions at similar points along their maturity curves, it is evident that the cost of singlemode networks has become more competitive to multimode. This has been enabled by transceivers that are optimized for data center applications. New multi-source agreements have produced PSM4 (4-pair parallel optics) and CWDM4 (duplex single-pair), which are excellent singlemode options for data centers like the hyperscalers build, needing longer (i.e. 500m) reach. The IEEE 100G-DR (single-pair) and 400G-DR4 (four-pair) standards are due early in 2018, and will also support short-reach singlemode options. Recently, Finisar announced an eSWDM4 transceiver that will support 400m over a single-pair OM5 cable. This narrows the reach difference between newer, low cost singlemode options and newer multimode options that also include four-pair SR4 and eSR4.

You can read more in our high speed migration white paper for more information on the array of data center optic applications and considerations for singlemode and multimode networks. In the meantime, what are you using to make the most of your network?

About the Author

James Young

James Young

James currently serves as the Director of CommScope’s Enterprise Data Center division, overseeing strategy and providing leadership to product and field teams globally. Formerly James has been involved in a variety of roles including sales, marketing and operations for communication solutions working with Tyco Electronics/AMP, Anixter, Canadian Pacific and TTS in Canada. 

James has gained extensive experience in the sale of OEM products, network solutions and value-added services through direct and indirect channel sales environments. His sales experience includes electronic transmission components, telephony systems, network systems, LAN infrastructure products and fibre transmission system products. James has garnered substantial experience in OEM and channel marketing, as well as network operations as assistant director of CP’s computers and communications group. 

James graduated with a Bachelor of Science from the University of Western Ontario.  He is a registered Communication Distribution Designer (RCDD) and certified Data Center Design Professional (CDCP).